1/28/2021 4:15 PM | |
Joined: 1/31/2020 Last visit: 10/11/2022 Posts: 19 Rating: (0) |
Hello! I faced the following problem when setting up the connection between "G120P CU230P-2 DP" and S7-1200 1215 DC/DC/Rly via Profibass DP, the fact is that I cannot turn on the frequency converter in automatic mode from the controller, and with manual switching on I can read data on the speed of the drive, tell me how and through which control word can you start the drive from the controller? I will attach the screen of the program to the message.
AttachmentScreen.pdf (73 Downloads) |
1/29/2021 6:34 AM | |
Joined: 1/31/2020 Last visit: 10/11/2022 Posts: 19 Rating: (0) |
|
Last edited by: Rabinio at: 01/29/2021 06:36:32 |
|
Follow us on