3/6/2023 1:17 PM | |
Joined: 9/8/2016 Last visit: 9/27/2023 Posts: 1 Rating: (0) |
Did anyone find a solution for this ? |
4/12/2023 7:23 AM | |
Joined: 1/23/2020 Last visit: 10/31/2023 Posts: 31 Rating: (6) |
Hi, maybe the name of the topic is a little bit confusing. I think what you are searching for is a possibility to delete files via the webserver via a program e.g. a batch file (without operating the browser manually). I don't have experience with the S7-1200 Webserver but I posted a topic about the S7-1500 Webserver: Curl Commands for S7-1500 Webserver. Because of the possibly different file structure in a S7-1500 I can not promise that the commands in the topic work analog with a S7-1200 webserver. But you can always copy the curl command(s) when you operate your browser manually (in the way you wish to automate further) as shown here: Copy as curl Don't forget that depending on your settings some operations (e.g. deleting, uploading, ...) require admin rights. Therfore you need to login e.g. via wget analog as shown in the topic about S7-1500 Webserver Curl commands. Regards |
This contribution was helpful to1 thankful Users |
Follow us on