2/10/2021 9:04 AM | |
Joined: 6/19/2017 Last visit: 4/19/2024 Posts: 7961 Rating: (162) |
Hi mmitton, thank you for reporting this issue to us! As a workaround for answering into the topic I suggest following options: - You create a suggestion in the topic, so that it can be converted to a post within the thread. You can find the "Suggestion" button next to the "To thank" button on a post. - You write your answer via a personal message to a Moderator, so that it can be moved to the proper topic. If you choose this option, please, also tell in which topic your message should be transferred. - You create a new thread, so that it can be transferred to the regarding topic. Also, if you choose this option, please mention in which topic you wanted to publish the answer. I'm really sorry for this inconvenience Best regards, |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
Follow us on