2/15/2021 11:31 AM | |
Joined: 3/11/2019 Last visit: 9/6/2024 Posts: 1569 Rating: (289) |
Dear Ilkka_L, in general the module can also measure resistance/resistors (2-,3,4-wired) , not only temperatures. There is also a parameter for resistance input range up to 6000 ohms, which would fit your requirement. Informations can also be found with following links. maybe this helps. SIMATIC ET 200SP analog input module AI 4xRTD/TC 2-/3-/4-wire HF-> "Input ranges (rated values), resistors" -> "Input resistance (0 to 6000 ohms)" Representation of analog values for resistance-type sensors regards sancruz |
Last edited by: sancruz at: 02/15/2021 11:33:00Last edited by: sancruz at: 02/15/2021 11:43:34Feedback appreciated, please rate |
|
This contribution was helpful to2 thankful Users |
Follow us on