3/26/2020 2:22 PM | |
Joined: 10/26/2017 Last visit: 2/17/2024 Posts: 1 Rating: (0) |
Hi guys, i'm in search for most basic example for reading and writing json file in plc 1511. Here is the code example, and what i must do is reading specific strings from file and saveing to the PLC, for example: PAA00000, 900000101.SNTTEST... and so on. After that, making my own json file with identical structure. The file I need to read and write is on a PC that is connected to the PLC via ethernet.
Attachmentjson.txt (389 Downloads) |
This contribution was helpful to1 thankful Users |
2/26/2021 10:28 PM | |
Joined: 9/24/2020 Last visit: 7/2/2022 Posts: 1 Rating: (0) |
Hello friend, did you manage to evolve with this theme? |
2/26/2021 11:15 PM | |
Joined: 7/7/2010 Last visit: 4/25/2024 Posts: 14628 Rating: (2348) |
Perhaps you can find suitable blocks to accomplish your task here: There may be other open source libraries available (like Siemens' library site: https://support.industry.siemens.com/cs/document/109738702
|
science guy |
|
Follow us on