2/20/2021 3:42 PM | |
Joined: 3/11/2015 Last visit: 6/25/2024 Posts: 68 Rating: (1) |
Dear all, Without enabling the Monitor keyboard(WinCC Explorer Onscreen keyboard) in the projects, the Title bar is visible on triggering the Keyboard via a button in Runtime, hence I could close the keyboard from close option available in the Title bar. But on enabling the the Monitor keyboard(WinCC Explorer Onscreen keyboard) in the projects, the Title bar is not visible, because of which couldn't close the keyboard. Kindly find the Runtime images with & without the Title bar for your reference. And kindly let me know whether it can be resolved & if yes then the solution to fix it. Regards, CoreGuy AttachmentOnScreenKeyBoardTitleBarImages.zip (130 Downloads) |
5/3/2021 4:45 PM | |
Joined: 3/11/2015 Last visit: 6/25/2024 Posts: 68 Rating: (1) |
Hello everyone, It seems the Title bar gets disabled on Enabling Monitor Keyboard. OS: Pre-requisite condition: 1)User Accounts > Change User Account Control settings > Choose when to be notified about changes to your computer" > "Never notify" setting Observation: Note: Application can be opened either by C Script or VB Script. Reference link for Command line parameters used in both C Script & VB Script: Reference link for closing an Application Window: https://support.industry.siemens.com/cs/au/en/view/2976503 Kindly find the attachment for the Scripts(with comments of Observations/ Testings), Images & Screens for your reference. Regards, AttachmentFinalWinCCOnScreenKeyboard.zip (154 Downloads) |
Last edited by: Jen_Moderator at: 05/04/2021 07:56:14Optimized link. |
|
This contribution was helpful to1 thankful Users |
Follow us on