5/19/2021 1:47 PM | |
Joined: 3/11/2019 Last visit: 4/26/2024 Posts: 1378 Rating: (244) |
Hi CPUSurfer, in the hw-config it is not possible to mix up siplus components with standard compontes. If you want to configure a siplus product, also the cpu has to be a siplus. As Daniel Chartier already mentioned, you can use also the standard product number for a siplus product, it should work if you use the product number of the standard component in the hw config, the siplus component is based of. How do you configure a SIPLUS extreme component with the TIA Portal?regards sancruz |
Last edited by: sancruz at: 05/19/2021 13:48:11Last edited by: sancruz at: 05/19/2021 13:52:11Feedback appreciated, please rate |
|
This contribution was helpful to2 thankful Users |
Follow us on