9/16/2010 11:08 AM | |
Joined: 6/1/2007 Last visit: 5/2/2019 Posts: 86 Rating:
|
Are you changing in module drivers? if yes, they are generated and will be generated again. Yer |
9/23/2010 11:08 AM | |
Joined: 5/27/2008 Last visit: 7/22/2018 Posts: 96 Rating:
|
Hiwolf08, The CFC is meant to automatically save all the changes you make. The only think that will cause this is if you are working in a auto generated CFC (used for driver blocks) or F blocks (safety matrix blocked, generated whenever you compile your safety marix) or if you update the process tag type. If this is not the case then can you please confirm which runtime group it is adding the blocks (the runtime group can be found out by clicking on the green box on the block) Hope this was helpful. If this does not help then please send some screen shots. regards, Minhaj
|
9/23/2010 8:47 PM | |
Joined: 7/8/2010 Last visit: 10/8/2014 Posts: 14 Rating:
|
hi minhajie, the one you are referring to is not my case, im not working with automatically generated cfc, and due to the nature of the problem is not possible to take a screenshot, i will try to explain itand i know its not suppose to happen because theres i no SAVE or UNDO in PCS7: i insert an OR block an rename it then i insert an AND block and rename it,the momenti try to connect the output of an already existing block (anyone) to the OR block a message appears "the block doesnt exist" and then both blocks dissapear (OR & AND blocks) like if i never did anything at all. This can happen after i did a lot of changes so is kind of frustrating. im receiving one message error continuosly that perhaps has something to do with the problem, i add a screenshot. any idea? Regards |
9/24/2010 12:05 PM | |
Joined: 5/27/2008 Last visit: 7/22/2018 Posts: 96 Rating:
|
Hiwolf08, If you don't want to do what Yer said then I would recommend you to close all application and do a system restart and then try one more time. It is a common practise but I though it is worth mentioning in case you haven'tdone it? regards, Minhajie
|
Follow us on