9/21/2019 5:01 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello Saleh; What do you mean exactly by the "pin assignment" of the IM 153-1? Are you enquiring about the pinout of the Profibus cable, the module U-Connectors? In any case, ot is highly recommended that you use Pofibus cables and connectors to link the Profibus slave (IM 153-1) and your Yokogawa master. This allows you to set termination resistors at both ends of the network, and takes care of grounding issues that can affect your transmissions, among other settings. Here, for initial information, is the manual for the ET 200M Profibus/Profinet distributed I/O system, including the IM 153-1: SIMATIC Distributed I/O device ET 200M https://support.industry.siemens.com/cs/ww/en/view/1142798 To setup an IM 153-1 and its I/O modules as a slave to your Profibus master, you mut integrate the ET 200M gsd file in your Profibus master's configuration software. The Yokogawa website mentions SyCon as their Profibus configuration tool. Read up on how to insert a gsd file so you can setup an external Profibus slave. In the following link you will find the gsd files available for the ET 200M family of distributed I/O; locate the correct part number of the IM 153-1 you are using, download the file and insert it in SyCon, as described in the SyCon manual. Then insert the I/O modules in the slave configuration so you can link these to the Profibus master memory and addresses. Note that you must use the IM 153-1 dipswitches to set the Profibus slave address on the interface module, and it must match the Profibus address attributed to it via SyCon. PROFIBUS GSD files : ET 200M https://support.industry.siemens.com/cs/ww/en/view/113498 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 09/21/2019 17:03:21 |
|
10/15/2019 11:24 AM | |
Joined: 8/16/2015 Last visit: 6/6/2022 Posts: 37 Rating: (0) |
Dear Dcharier, Kindly i did configuration via Sycon Putting GSD file of IM 153-1 , configure slave address ... etc. and connect the IM 153-1 and NFLP 121 together by Profibus cable with two connectors with Part No. (6ES7-972-0BA20-0XA0) but when i connect the communication cable BF led of IM module flashing and the communication not established (Note that i need to establish the communication for IM module as slave without any connection to Siemens CPU ) Regards, Saleh
|
10/15/2019 3:41 PM | |
Joined: 8/16/2015 Last visit: 6/6/2022 Posts: 37 Rating: (0) |
Dear Dchartier, Kindly find the attached Sycon Conf. and IM153-1 Conf. Regards, Saleh
AttachmentSycon_conf_&IM153-1.zip (282 Downloads) |
11/4/2019 1:10 PM | |
Joined: 8/16/2015 Last visit: 6/6/2022 Posts: 37 Rating: (0) |
Dear dchartier, Kindly i am already online but Diagnostic Menu still dummy ,on the other hand may be the GSD file version effect the establishment of communication .as per the attached file the IM 153-1 version is 1.7 but i didn't find the GSD file with Rev 1.7 on Siemens forum link https://support.industry.siemens.com/tf/ww/en/posts/problem-with-et200-profibus-communication/20503?page=0&pageSize=10 Regards, Saleh
|
Follow us on