Industry Online Support
Technical Forum
4/5/2013 8:56 AM | |
Joined: 8/31/2010 Last visit: 9/22/2024 Posts: 1521 Rating: (227) |
Hello pyrovo, What is the firmware of the CPU 1214C you are using? Try using the following options and find out the icon of your block, if it is not green then scroll through that complete program block to find out if there is any difference in online and offline code. If it is showning only a Green icon then try to compile the whole CPU and downloaded all blocks again? Otherwise perform a factory reset and then load your complete program to check if this is solved, before performing a factory reset - beware on what happens to the CPU after reset - Resetting to factory settings |
Like it? Rate it! |
|
4/5/2013 6:34 PM | |
Posts: 40 Rating: (0) |
Try to fo offline and do compile all. |
Last edited by: Dob at: 4/5/2013 6:34 PM |
|
4/8/2013 11:07 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is discussed in the following thread,too. s7-1200 compare blocks problem Best regards O_Moderator |
This contribution was helpful to1 thankful Users |
Follow us on