7/18/2018 4:21 PM | |
Posts: 146 Rating: (7) |
I have Advantech EKI-1521 Gateway module. I need to connect it to S7-1500 CPU over Ethernet port. On other side of EKI module is Modbus RTU device. How do I access Modbus RTU device registers over EKI module? Is it Modbus TCP/IP server for S7-1500 side? Or do I need to use TSEND and TRECV functions in order to establish communication? BR, Milos ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/19/2018 6:39:51 AMNew subject after splitting |
|
7/19/2018 3:28 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (819)
|
You're welcome Milos. |
With best regards... |
|
Follow us on