5/3/2015 11:00 PM | |
Joined: 11/7/2012 Last visit: 3/24/2020 Posts: 67 Rating:
|
Normal
0
false
false
false
EN-US
X-NONE
AR-SA
MicrosoftInternetExplorer4
Hi Mike, I have connected this 7XV Module to a Siprotec device (7SJ621) in both PRP and Line mode and with or without switch in between, I could manage to ping the device and open it in IEC browser. The issue is GOOSE massage is not working as I expected! I use CTRL/GGIO01/Ind0x as source but it is invalid point in IEC browser! (Image No. 3) The LN that is actually changing due to the change of Module inputs is CTRL/ctlGGIO01/SPCSO0x (Image No. 2) which is not available in to use as source in IEC 61850 Station. I attached some screen shots for more clarification and ICD and MAP file of one 7XV56 Module. Thanks again for your support AttachmentMAP.rar (37 Downloads) |
Follow us on