(0)| 5/26/2014 10:45 AM | |
|
Posts: 1368 Rating:
|
Hello, if i remember me, the ex282 is protocol "Ethernet powerlink" and the CP343 "Ethernet TCP/IP". So you need a Gateway between these modules... for example http://www.hms.se/technologies/powerlink.shtml Greetings |
| 5/26/2014 12:29 PM | |
|
Posts: 61 Rating:
|
hello Pittiplatsch actullay there is running system and harware configuration is B&R powerpanel 4pp220 is communcation with ex282. i need to access the data of analog module attaced with ex282 on WINCC. 1st option was that i use cp343 and gateway to access that analog channel of ex282. is there any opc server which allow me to receive the data on wincc directly ?via ethernet powerlink |
Follow us on