5/16/2019 9:44 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Hello Yellowbeard, I suspect your AS-OS connection dropped. Click on the AS2 User project, then click on the Netpro editor (See attached picture). Then look for your PLC, click on the CPU, there will be S7 connections between your OS station to your AS station. RIght click on those s7 connections and Download selected connection. Complete guideline on netpro, you can refer to Engineering System V9.0 SP1 Section 9.14, Page 424 , Points to note when downloading. Then you can search "Netpro" to understand more on the netpro editor. |
Last edited by: Jen_Moderator at: 05/16/2019 14:23:27Optimized link. Please give me 5 stars Rating if my post is helpful for you. :) |
|
5/16/2019 2:03 PM | |
Joined: 6/26/2018 Last visit: 4/16/2024 Posts: 43 Rating: (0) |
Hello Dear Expert, l opened Netpro and select Cpu then dowload project. now l don't see error" Connection AS' not established". But l see " Read Error I/O devices :FC2548 addr:432" and Wincc still red things. By the way ET200M has no power. l added 2 photo . One is error photo other is wincc red things photo. Best Regards AttachmentError and wincc photo.zip (61 Downloads) |
5/16/2019 3:05 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear Yellowbeard, Can you check something? 1. Wincc Explorer of OS Server (Master), at the menu bar - > Tool - > Driver Status , server status. Take a picture of them. 2. At the WinCC explorer, Double click Tag Management, At the Name connection or industrial Ethernet , Take a picture on them.. These are to check whether your connection to AS2 established or not. The Address issue is separate issue. we can analyse them in different post. |
Last edited by: JazTai at: 05/16/2019 15:05:38Please give me 5 stars Rating if my post is helpful for you. :) |
|
5/17/2019 8:11 AM | |
Joined: 6/26/2018 Last visit: 4/16/2024 Posts: 43 Rating: (0) |
Dear JazTai l sent you these document. Best Regards Attachmentİmages.zip (52 Downloads) |
5/17/2019 8:40 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
For the IMG_7835, which station you taken at? Can you double check at the both of the OS server? it should have a small green color tick there to show AS connection established. For the IMG_7836, can you check at your OS Client Station? the status of Driver / server connection should not greyed out. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
5/17/2019 11:40 AM | |
Joined: 6/26/2018 Last visit: 4/16/2024 Posts: 43 Rating: (0) |
Dear expert, l took photo from master server and added photo in attachment. Best Regards AttachmentPhotos.zip (49 Downloads) |
5/17/2019 12:08 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear Yellowbeard, From what I see in IMG_11, your AS2 has established. You have a different issue now. Probably you do these: 1. Close this thread and create another one. 2. Mention the alarm message. 3. Check the grey out tag, see what is the tag behind. 4. Take a picture on the Function block in simatic manager, look for the FB number in the block folder and in the charts you are using. Hope this is helpful for you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to2 thankful Users |
Follow us on