6/30/2006 9:21 AM | |
Joined: 8/31/2005 Last visit: 7/24/2024 Posts: 217 Rating: (41) |
Hi! Maybe this will help you: |
Greetings, Chris |
|
3/16/2009 9:49 AM | |
Posts: 8 Rating: (0) |
The first link is not working anymore. Has someone the working link? |
3/23/2009 11:56 AM | |
Posts: 22 Rating: (2) |
Hi this program can do it for you. Her it is yoused in SCL: // Make Time as DT to String DTConvert.TimetoWinCC(Dato := "CPU-Watch".ActPLCTime, Trig := TrigFB); "StrtRWay".RWay[Index].Start := TimetoWinCC.DTString; // OUT: STRING AttachmentFB342.ZIP (1238 Downloads) |
This contribution was helpful to1 thankful Users |
8/19/2019 8:22 AM | |
Posts: 17 Rating: (6) |
Here is a piece of code i wrote in SCL to solve this issue, rename the text file to .scl and import the code in your project, Cheers, AttachmentDT_TO_STRING.txt (1353 Downloads) |
This contribution was helpful to5 thankful Users |
1/15/2020 4:46 PM | |
Joined: 6/16/2015 Last visit: 1/31/2022 Posts: 1 Rating: (0) |
Thank you That's what I need! Works! |
1/8/2024 11:35 AM | |
Joined: 5/20/2021 Last visit: 4/9/2024 Posts: 1 Rating: (0) |
Top notch, perfect for what I required. Thank you |
Follow us on