9/15/2016 8:08 AM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Yes! What you are looking for is chart-in-chart technique. Follow these steps: 1. Open a CFC chart 2. Right click and select: "Insert new chart". 3. A empty block is added in your CFC chart... 4. Right click and select: "Open" 5. Create your desired functionality by adding blocks from the library 6. Create the necessary inputs and outputs by going to View->Chart IOs. You can see now a list with IN, OUT and IN_OUT. In there you can create your inputs and outputs. Don't forget to add your system attributes such as "S7_m_c" (OCM capable parameter) and others. You can do that by selecting an IO, right click->Object Properties->Tab: "Attributes". 7. Exit the CFC chart after adding your IO. 8. Now you have created a chart in a chart and you can use this multiple times as you wish. Good luck! |
Last edited by: Oreca at: 9/15/2016 8:13:24 AMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to4 thankful Users |
Follow us on