2/19/2018 6:11 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hello, update the Firmware on the CF on the CU320-2 PN. https://support.industry.siemens.com/cs/ww/en/view/109740193 https://support.industry.siemens.com/cs/ww/en/view/109751474 Regards |
This contribution was helpful to1 thankful Users |
2/19/2018 9:31 AM | |
Posts: 137 Rating: (0) |
Hi, It must be updated via Hardware CF card? Right? Thanks |
2/19/2018 10:11 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hello, no for S120 no FW V4.5 available (no HSP or something like that) so you can only use V4.8 or V5.1 FW Version. the procedure for a FW Update with the integrated Webserver in the CU320-2 is descriped in the Function Manual of sinamics https://support.industry.siemens.com/cs/ww/en/view/109754299 Regards Christoph |
3/8/2020 7:19 PM | |
Joined: 3/7/2020 Last visit: 9/1/2021 Posts: 1 Rating: (0) |
4.8 записать версию 5.1SP1 и использовать ключ от версии 4.8 |
3/9/2020 6:04 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Please use english language! |
Follow us on