6/21/2018 4:43 PM | |
Joined: 3/30/2015 Last visit: 3/7/2024 Posts: 70 Rating: (1) |
Good day all, Please i have a similar issue "Unable to Copy block" When I click details i see " (D280) Error compiling block in S7-300 CPU. I have like over 25 blocks that refuse to download to the PLC. I am using a PLC 317 -2 PN/DP and I have various bus faults and System faults on the various SM modules on the field. I have attached the CPU error message. I am using timers tagged "T1000", T1001", "T1002" etc. in one of the blocks that refused to download. How can i check if I am exceeding the CPU memory or how can i expend it? Regards, David ------------------------------------------------------------------------------------------ AttachmentDiagnose.txt (121 Downloads) |
Last edited by: Jen_Moderator at: 6/22/2018 10:09:20 AMNew subject after splitting |
|
6/21/2018 4:44 PM | |
Joined: 3/30/2015 Last visit: 3/7/2024 Posts: 70 Rating: (1) |
This is sample code in one fo the blocks that refused to download. Thanks. David |
1/24/2020 11:50 AM | |
Posts: 1 Rating: (0) |
Hello, The program was developed in S7 for CPU 315-2 and Working fine and now trying to use CPU- IM151-8 PN/DP (6ES7151-8AB01-AB0), while trying to download error occur (D280 Error compiling block in S7-300 CPU ) Kindly suggest how to solve. With regards, shabu
|
Follow us on