2/8/2010 4:16 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hello, can you post the diagnosticLog of the D425. Normaly it logs why the CPU goes to BZ STOP. Regards Christoph |
2/9/2010 9:29 AM | |
Posts: 16 Rating: (0) |
Hello Christoph I uploaded a log-file and a doc-file with 2 screenshots on the error. We also integrated a PROFINET communication (PLC = IO-controller, D425 = IO-device) and this works fine. But the problem on PROFIBUS persists. In the log-file, specifically event 5 looks to give the error information, but it doesn't really provide a solution. Can you help me with that? Thanks in advance, kind regards Stijn AttachmentD425_error.zip (174 Downloads) |
2/15/2010 9:37 AM | |
Posts: 16 Rating: (0) |
Dear Christoph In attachment I uploaded the program which runs in the background task and which deals with the PROFIBUS communication. In the last network I used both options 'When_Command_Done' and 'Immediately' for the parameter 'nextcommand'. If you want I can upload the archived project in Simotion scout. Do you consider any changes? Can I run this program in a motion task? What do I have to use as a startcommand for that motiontask? Thanks in advance, kind regards Stijn AttachmentSIMOTION_SCOUT_document.pdf (203 Downloads) |
Follow us on