11/13/2012 6:53 AM | |
Joined: 10/7/2005 Last visit: 9/23/2024 Posts: 3022 Rating: (1054)
|
Hello Saga
easy one first: What properties, advantages and special features does the ISO protocol offer? What properties, advantages and special features does the ISO-on-TCP protocol offer? What properties, advantages and special features does the TCP protocol offer? What properties, advantages and special features does the UDP protocol offer? What properties, advantages and special features does the S7 protocol offer?
the only meaningful answer I can give, is that you select the one that is most suitable for the given application. The above links will already tell you the main advantages and disadvantages of each and the compendium below shouldhelp too with the selection: CPU-CPU communication with SIMATIC controllers (compendium) I hope this helps |
Cheers |
|
This contribution was helpful to3 thankful Users |
Follow us on