11/25/2014 5:16 PM | |
Posts: 19 Rating: (0) |
I have also tried the attached but no acessable nodes are detected
AttachmentHow to setup Teamviewer VPN.pdf (737 Downloads) |
11/25/2014 5:19 PM | |
Posts: 5225 Rating: (1185) |
Someone at some point was mentioning something about port-forwarding. |
11/25/2014 5:54 PM | |
Posts: 19 Rating: (0) |
Can you explain please? |
11/25/2014 7:31 PM | |
Posts: 5225 Rating: (1185) |
This is all I have..[LINK] |
11/27/2014 8:41 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello, for the download of an updated Code for STEP 7 (TIA Portal) you need the software in this regard. Please find also the information in the FAQ: http://support.automation.siemens.com/WW/view/en/42637263 With best regards |
11/27/2014 9:09 AM | |
Posts: 5225 Rating: (1185) |
Thank you for the suggestion.. However the real question is not for making a download while you are "close" to the PLC. It is not about local download; it is about "remote" work: TIA PORTAL >>>>> INTERNET LINK >>>>>> PLC The answer is port forwarding.. but that is all I know. Greetings. w |
11/27/2014 10:10 AM | |
Posts: 5225 Rating: (1185) |
Thanks for that idea. There might be another option. The newest Siemens Automation Tool [LINK] has the ablity to download a program to the S7-1200 without having TIA Portal installed. I have tried it once for testing on a previous update of the current version. It works a little bit strange.. and I can't remember all the steps. You prepare the downloadable file with TIA by "downloading" via your SD card reader to a (normal) SD card. The file that is created on the SD card can then be sent to your client. The client uses Siemens Automation Tool to load the file into the PLC. - - or something like that. Greetings. w |
11/27/2014 10:20 AM | |
Joined: 12/16/2012 Last visit: 4/19/2024 Posts: 651 Rating: (129) |
Hi! Now that you mention it, I remembered reading a post about it: |
Follow us on