1/14/2011 12:28 PM | |
Posts: 27 Rating: (1) |
Hi Timmy, iam also facing the similar problem of Drive CliQand i created a new thread yesterday "Drive Cliq Error"as follows: Did you find the solution? If yes please share the solution. Thank you. Dear Expert,
Observation: One of the 4 MoMo goes into not ready state(inferred by the red led indication in MoMo) while the other 3 are healthy. Splitted from Fault F30008. |
Last edited by: O_Moderator at: 1/14/2011 2:10 PMnew subject after splitting |
|
1/14/2011 2:11 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already published in the following thread Drive Cliq Error!!!!!!!. Best regards O_Moderator |
Follow us on