1/16/2016 8:36 PM | |
Joined: 12/7/2011 Last visit: 6/21/2024 Posts: 384 Rating: (9) |
Hi to all, I've one problem with an error coming form the trend Archive: The system is WinCCflex 2008 sp3 and a touch panel MP 377 Trend configuration in the Historical data is: 100 data log, one for each variable Number of data records per log = 500000 Storage location = File - CSV (ASCII) Path = \Storage Card USB\ Logging method = Create segmental circular logs automatically Number of logs = 8 Each varible is linked to one data log, and for the trend configuration i've used this example: The problem is that after load the project, in a trend view i don't see noyhing and in a diagnostic view appear: Archive tagxy is corrupted. I soo in the MP377 that there's some limitation and i try do convert the configuration according the manual, but without succes, i also try to delete all and configure only one variable but the proble is still present. Please someone could help me? Regards Duccio.
AttachmentError.pdf (274 Downloads) |
Last edited by: Duccio at: 1/16/2016 8:39:59 PM |
|
1/18/2016 5:05 PM | |
Joined: 12/7/2011 Last visit: 6/21/2024 Posts: 384 Rating: (9) |
Hi Murof, Thanks for your reply.
It seams that you cannot access the Storage card or USB Stick. Exactly, the strange thing is that after restart of the panel, the Trend view seams to work properly, but after a few seconds is stopped, and even the alarm history desappear . But i don't understand what you mean when you said:
set the Log to the deifferent Message classes in Message Class editor. Wich message calss editor you mean? Is the Alarm Class message editor? Attachmentlog.pdf (170 Downloads) |
1/19/2016 5:30 PM | |
Joined: 12/7/2011 Last visit: 6/21/2024 Posts: 384 Rating: (9) |
Hi Murof, Don't warry we are already busy with the work and it's possible to make a mistake! But I'm very confused, because the same project loaded in the panel, with only one tag, i've changed it in WinCC runtime and start in my laptop and work properly. Please Heeelp!!! AttachmentPanel.pdf (177 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on