1/2/2013 12:58 PM | |
Posts: 836 Rating: (99)
|
Hi, did you solve this problem? |
1/11/2013 7:01 PM | |
Posts: 4 Rating: (0) |
No, this problem has not been solved. In fact, today I made an archive of my PCS7 project, brought it to another ES. Upon compiling the OS or running the WinCC portion of PCS7 iget the same pop-up telling me an internal error has occurred and that I need to restart. These machines came directly from Siemens and have not had an outside connection to the web so I am pretty sure viruses are not to be blamed. Any thoughts? Thanks |
1/12/2013 8:13 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (927) |
I doubt it will be 100% solution, but you can try to archive with reorganization...Seems it is inside the project, not on the computer. Affter that doesnt help, I think you can try to copy the project to a new one...Takes some time, but you be able to save your project....i hope... |
If I could help you, you can use the RATE button. Thank you. |
|
1/16/2013 3:26 PM | |
Joined: 1/15/2009 Last visit: 4/19/2024 Posts: 316 Rating: (40)
|
After trying the Save As with Reorg (which is a good next step from Oreca), it might be worth seeing if other OS applications have issues on the ES. Try creating a new project through the Project Wizard and see if there is an issue creating a new OS application, or error on OS Compilation. Its a little bit of an effort, however if the system cannot do this, there might be a problem with the software load. Have a great day.
|
The best location for all PCS 7 content (manuals, guides, application notes, FAQs, and videos). |
|
4/20/2016 9:27 AM |
|
Joined: 12/14/2015 Last visit: 10/25/2022 Posts: 9 Rating: (0) |
Note that WinCC is not allowed on domain controller... |
3/12/2023 3:00 PM | |
Joined: 3/5/2014 Last visit: 4/12/2024 Posts: 29 Rating: (0) |
Did you solve this problem? |
Follow us on