7/26/2006 10:27 AM | |
Posts: 17 Rating: (0) |
Hi, I have Simatic Step 7 Version:V5.3 + SP2, Revision Level K5.3.2.0 installed on my PC. While writing code in the LAD/STL/FBD Programming Block window, it closes without saving after showing error message. I have enclosed the snapshot of the error message. Regards, AttachmentError in Step7.zip (592 Downloads) |
7/26/2006 10:58 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147) |
Hello, Before the error pops up, what did you do? Is it only in one project or in all projects? Best regards, Wizard |
7/26/2006 12:27 PM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147) |
Hello, Perhaps the following will help: Workaround: in the supplement you find two Reg-files to enable and disable this function. You have to disable the functionality in order to avoid this behavior.
Best regards, Wizard AttachmentXMLCopyPaste.zip (606 Downloads) |
7/26/2006 2:18 PM | |
Posts: 17 Rating: (0) |
Thank you Wizard, I have run the file and the problem is resolved. Thank you again. Regards, |
7/27/2006 8:49 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147) |
Your welcome, Greetings Wizard |
8/1/2006 9:42 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147) |
Hello Late, I got it from the Siemens Hotline. Best regards, Wizard |
Follow us on