Industry Online Support
Technical Forum
6/7/2017 11:58 AM | |
Posts: 1 Rating: (0) |
Hi. I have an error (Micro/Win v4.0.9.25): Masters exist on the PROFIBUS network and the current device does not support masters. Try again after selecting a multi-master device. How do I upload from PLC? I can not the PLC to STOP. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/9/2017 4:11:32 PMNew subject after splitting |
|
6/10/2017 11:05 AM | |
Posts: 5 Rating: (0) |
if the HMI is the only master in the network,power off the HMI,then you can upload the pragram,it won't stop the cpu |
Follow us on