4/6/2016 5:12 PM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
Dear Gents; While I was proposing a new system architecture for PCS7, I found that I could use ET200SP as a process remote I/O. I was wondering if any body used it in a large scale project. I found a link for the reference projects of ET200SP here, but for large PCS7 I need your references. |
Best Regards |
|
4/25/2016 12:51 PM | |
Joined: 10/26/2011 Last visit: 5/3/2024 Posts: 761 Rating: (190)
|
Hello, ET 200SP is a released component for PCS 7. See the manual "SIMATIC Process Control System PCS 7 Released Modules", chapter 8. https://support.industry.siemens.com/cs/ww/en/view/106210481 |
SIMATIC PCS 7 - Overview |
|
4/25/2016 1:07 PM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
Hi Thunderstorm; Thanks for your reply. I was wondering if this thread was not seen by any of the forum members I know that ET200SP is a released component of PCS7, But I was asking if any one could share his experience of using it in a PCS7 project.
|
Best Regards |
|
4/25/2016 1:08 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928) |
Hello, It is basically the follow up of ET200M. For now, the ET200SP is only available in a Profinet network, not yet for Profibus. |
If I could help you, you can use the RATE button. Thank you. |
|
4/25/2016 1:30 PM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
Thanks Oreca for your contribution.
I thought that ET200MP is the follow Up of ET200M. Check this link
That is correct. For PCS7 it only supports Profinet IM not Profibus IM, although ET200 SP as a remote I/O supports both: SIMATIC ET 200SP - Interface Modules and BusAdaptersThe ET 200SP is connected to the bus system via the interface module. Either PROFINET interface modules or PROFIBUS interface modules can be selected. The interface module exchanges data between a higher-level controller and the I/O modules. Interface modules to PROFINET With the PROFINET interface module, the variable BusAdapter can be easily plugged into the interface module, which allows the connection technology via PROFINET to be freely selected. The following versions for connecting to PROFINET are available: IM155-6PN Standardincl. server module IM155-6PN Standardincl. server module and mounted BusAdapter BA 2xRJ45 IM155-6PN Basicincl. server module with 2 integrated RJ45 sockets IM 155-6PN High Feature Interface module to PROFIBUS With the PROFIBUS interface modules, the DP connector is a PROFIBUS connection via a 9-pin sub D socket. The following module is available for connecting to PROFIBUS: IM155-6DP High Feature
|
Best Regards |
|
4/25/2016 3:28 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928) |
Hello Khaled, Hmm, I thought the ET200MP is mainly used for S7-1500 systems. See attached... Attachmentdffa-b10140-00-7600.pdf (93 Downloads) |
If I could help you, you can use the RATE button. Thank you. |
|
4/25/2016 6:37 PM | |
Joined: 10/26/2011 Last visit: 5/3/2024 Posts: 761 Rating: (190)
|
I am not involved in the engineering and project planning. But I have found an interesting App in the App Stores (Apple, Androis). This app called"Siemens Industry References" and gives you an overview of different reference projects. Sorry, I didn't have a look, if some projects using ET 200SP. Android Store: Apple Store: |
SIMATIC PCS 7 - Overview |
|
Follow us on