(1)| 7/24/2015 11:32 AM | |
|
Posts: 1058 Rating:
|
Hello jankoslayer, yes, there are HW modules for communication with Siemens via profibus: regards
|
| 7/24/2015 11:53 AM | |
|
Posts: 160 Rating:
|
My bad... sorry. I wanted to ask if there are hw modules for POWERLINK comunication for SIEMENS... I'm gonna edit my first post right now. Janko |
| 7/24/2015 1:08 PM | |
|
Posts: 1058 Rating:
|
I dont think that there is hw module that supports a connection via POWERLINK. You can use a CP343 for communication with Ethernet TCP/IP, but not directly for POWERLINK. See also here: connecting B&R ex282 powerlink bus controller with s7-300 regards
|
This contribution was helpful to
|
|
| 7/25/2015 12:16 PM | |
|
Posts: 160 Rating:
|
Hi, I found out this module EX282 B&R. Obviously it's likely that I'll need cp343 + some king of gateway between them. And here I have a problem because I do not really know what to use as gateway. Do you have any idea what to use? I'll tell you more, I even do not know if gateway is a physical module or a program or whatever it is... Regards, Janko |
| 7/29/2015 9:02 AM | |
|
Posts: 160 Rating:
|
Hi Mr, thank you for your reply. Now I have a big picture what I'm suppose to do! But I have one doubt. Looking at the CP343-1 datasheet, it clearly saying that CP343 is used for allowing S7-300 to connect on Industrial Ethernet. Datasheet of CP343 that I found is: CP343-1 Now, the question is: do I need CP343 if I use CPU 317-2 PN/DP which already has Industrial Ethernet connection integrated? I used this connection for establishing the connection with B&R CPUs by the way. Thank you in advance, Janko |
Follow us on