10/30/2017 1:15 PM | |
Joined: 5/9/2015 Last visit: 2/5/2024 Posts: 81 Rating: (4) |
Hello Oreca, Can you please provide the example program for the integration of Danfoss drive in the PCS7 project. Best regards, nkr ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/3/2017 9:44:12 AMNew subject after splitting |
|
10/30/2017 1:30 PM | |
Joined: 9/27/2006 Last visit: 5/1/2024 Posts: 12257 Rating: (2666) |
Hello nkr; Which model of Danfoss drive are you using in your project? Do you program your CPU wih TIA Portal or Simatic Manager? See the large amount of threads on the subject of Danforss drives and Profibus-DP from the forum pages: Youy will need to download the correst gsd file for your Danfoss drive, search for it on the Danfoss site, in their Fieldbus configuration files page: http://drives.danfoss.com/downloads/fieldbus-configuration-files/#/ In the same page, open the Documents.. link and search for Profibus documents, you will find good Installation and Application files for Profibus with the different Danfoss drives. Hope this heps, Daniel Chartier |
10/27/2021 12:51 PM | |
Joined: 1/29/2013 Last visit: 1/30/2024 Posts: 7 Rating: (5) |
Hello Naresh Saini Siemens offers a service for the integration of third-party devices in PCS7. To my knowledge are there different libraries for Danfoss. Partially even the maintanance station is supported and there are also other faceplates available. Try it best by e-mail. function.blocks.industry@siemens.com PS: With the purchase of licenses also a 5-year service contract incl. updates and support is included.
|
Last edited by: AutoGen_679887 at: 10/27/2021 12:52:00Last edited by: AutoGen_679887 at: 10/27/2021 12:54:19Last edited by: AutoGen_679887 at: 10/27/2021 13:18:41 |
|
11/18/2021 8:46 PM | |
Joined: 5/16/2016 Last visit: 4/19/2024 Posts: 41 Rating: (7) |
I attached screenshots of my project for Danfoss FC-302 VFDs, I use the FbDrive block which is available in PCS7 APL 8.0 and higher. I use Profinet for the connections. Note the following
|
Last edited by: Jen_Moderator at: 11/19/2021 10:43:42Optimized link. Why you troubleshoot? |
|
1/18/2022 1:49 PM | |
Joined: 1/29/2013 Last visit: 1/30/2024 Posts: 7 Rating: (5) |
Here's a link for the libraries. |
Last edited by: AutoGen_679887 at: 01/18/2022 13:52:42 |
|
9/16/2022 8:34 AM | |
Joined: 5/9/2018 Last visit: 4/30/2024 Posts: 2 Rating: (0) |
Thnx for Exapmle. Does it reads out the Current and the Power on FBDrive? If the Standard Telegram1 (for Danffos only STelegram1 is available) has only 2Words IN and 2Words Out. |
Last edited by: AutoGen_9593652 at: 09/16/2022 08:35:55 |
|
Follow us on