3/11/2012 6:25 PM | |
Joined: 8/31/2010 Last visit: 4/14/2024 Posts: 1509 Rating: (222) |
Hello angmu, You can use 6ES7290-6AA20-0XA0 (SIMATIC S7-200, EXPANSION CABLE FOR EM OF THE 22X CPU 0.8 M). This flat-ribbon cable can be used for the connection between CPU and I/Oexpansion module or I/O expanstion module to I/O expansion module. But still i'm not sure if you can use two of these cables in a single system. |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
Follow us on