8/3/2018 12:05 PM | |
Posts: 44 Rating: (0) |
Hello As attached video , could any one guide me what is the fault , and what is the possible solution for fixing ? What I have done : 1-I turned off the left cpu , remove the RAM , wait for about 2 minutes , after that , insert the RAM again and turned on the cpu , but still all leds are flashing . 2-I turend off the cpu , remove the RAM , then turned on the cpu without RAM , But still I saw the all leds are flashing . It will be correct by Re-downloading configuration program on faulty cpu ? Whats the possible suggestion for fixing this problem ? Thanks Attachmentvideo file.zip (145 Downloads) |
Last edited by: hossein82 at: 8/3/2018 12:06:22 PM |
|
8/4/2018 6:05 AM | |
Posts: 44 Rating: (0) |
Hello What do you mean about power cycle in the sentence "Just remove batteries and power cycle" ? When the PS be turned off , if I remove the batteries , it doesn't matter for the program that saved on memory or RAM ? Also it not possible to connect Faulty cpu (Left one ), I think it is because of the module CP443-1 (Attached video). For diagnostic buffer file , is it needed to press update button when the related window is open ? Thanks Attachmentbandicam 2018-08-04 08-20-12-378.zip (170 Downloads) |
8/4/2018 9:31 AM | |
Posts: 44 Rating: (0) |
AttachmentWorking cpu -Diagnose.txt (185 Downloads) |
Last edited by: hossein82 at: 8/4/2018 9:31:43 AM |
|
8/6/2018 9:48 AM | |
Posts: 44 Rating: (0) |
Hello I removed the batteries according you said and did your steps , The result : The blinking of leds are finished , then the CPU went in stop mode .After about 3 minutes , the CPU statues changed to run mode automatically , and now bothCPUs are run (attached picture & video ) As you see in the picture , there is fault on both cpu and i think it is because of some nodes that are off . Please answer 2 questions : 1) According to video and picture attached ,are the CPUs in redundancy mode ? 2) Why the CPU fell in fault ? Is it possible to happen again ? Thanks Attachment1.zip (189 Downloads) |
Last edited by: hossein82 at: 8/6/2018 10:59:36 AM |
|
Follow us on