8/8/2016 9:21 AM | |
Posts: 2 Rating:
|
Dear Colleagues, I am having faults on my Profibus network, consisting of a fiber optic ring with several OLMs, and drops off each OLM are Supermicro softPLCs (CP Card). The network consists of 12 Nodes & the distance between each OLM is ~10meters I checked the installation: Copper cables, connectors all found to be good. There are no power cables or VFD drives is the vicinity of the Profibus cables. I connected up the Profitrace adapter to analyse & found reqular station loss & retries on several devices. Each drops from the OLM is more than 2 meters. In Profitarce Software, what i did notice was the transmission speed, set at the maximum of 12MB/s. I dont think it is nescessary to run at that high rate & this may be the cause of these comms faults. Is it ok to reduce the speed to 1,5MB/s? How do i determine what is best for this control system? Can somebody assist me? ------------------------------------------------------------------------------------------ AttachmentSZMS - Profitrace Report - 8 August 2016.pdf (192 Downloads) |
Last edited by: yknott at: 8/8/2016 9:21:23 AMLast edited by: Min_Moderator at: 8/8/2016 2:57:23 PMNew subject after splitting Last edited by: yknott at: 8/9/2016 6:10:03 AM |
|
Follow us on