1/16/2012 5:37 AM | |
Posts: 11 Rating: (0) |
Dear Colleagues; Please find enclosed the Single line drawings for more information. Attachment8062_APPM_PM 6_DRY END_AS BUILT.pdf (261 Downloads) |
1/16/2012 11:14 AM | |
Posts: 11 Rating: (0) |
Dear Deep; 1) The Thyristor Model is MCC21-16IO8B Make: IXYS; The data sheet is enclosed. 2) Motor Field current is 6.3A and Resistance is 25.6 Ohms. 3) Field to Armature and with respect to ground is 200 M.ohms 4) Power Interuption occurs aproximately once in a month. Moreover Field Circuit failure occurs at the time of1) Power failure when machine is running smoothly or when we 2) restore the power regards Attachmentdatasheet.pdf (210 Downloads) |
Last edited by: sanjaywani7 at: 1/16/2012 12:40 PM |
|
Follow us on