Industry Online Support
Technical Forum
6/28/2011 9:15 PM | |
Posts: 15 Rating: (0) |
Dear All, 1.I have developed software in PCS7. While checking for Position feedback(Analog signal)for the valve i am getting the overflow value and underflow value as well as per the attachment. Position feedback is change in resistor with range of 0 ohm(0 % Position open)to 1 Kohm(100% posn open) 2.Ihave configured in hardware as R and range i have selected is 6Kohm. (There are only two range i.e 600 ohms and 6 k ohm and i have selected 6 Kohm as the range to measure is 0 ohm to 1 kohm). But i am getting abnormal value -327648 and 327648.. Kindlu give me some solution. AttachmentAbnormal_value_analogsignals.zip (97 Downloads) |
6/29/2011 8:53 PM | |
Posts: 15 Rating: (0) |
hi all, |
Follow us on