1/29/2018 12:54 PM | |
Joined: 10/13/2014 Last visit: 3/1/2023 Posts: 14 Rating:
|
hi everyone, I'm trying to create a project with PCS 7 .But when i use the S7 300 station i have difficulty to add the S7 300 elements. It used to show an error as you can see in the attached file. Thank for your help
AttachmentDoc1.pdf (157 Downloads) |
1/30/2018 11:26 AM | |
Joined: 10/26/2011 Last visit: 7/22/2024 Posts: 762 Rating:
|
Hello Samal79, the 300 CPUs are not released for PCS 7. Please have a look in the manual "PCS 7 Released Modules" For integration S7 300 CPUs in a PCS 7 project, you can use the Industry Library (IL)https://support.industry.siemens.com/cs/ww/de/view/109750809 Please note, this is only a implementation, you cannot use most auf the PCS 7 functionalities and features. For PCS 7 it is highly recommended to use CPU 410 (or the 400 CPUs, listed in the manual released modules). |
Last edited by: Thunderstorm at: 1/30/2018 11:34:49 AMLast edited by: Thunderstorm at: 1/30/2018 12:51:19 PMSIMATIC PCS 7 - Overview |
|
2/5/2018 10:14 AM | |
Joined: 10/13/2014 Last visit: 3/1/2023 Posts: 14 Rating:
|
Hi Thank you for your answer. I forgot to choose the standard profile in HW config it was configured on PCS7. As you can see on the attached document Best regard.
AttachmentDocument1.pdf (175 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on