10/4/2019 10:55 AM | |
Posts: 1 Rating: (0) |
Hi sir using s7- 1200 i have to write values to external device register (40000---) in MODBUS TCP/IP communication. currently that devices as works as a Master .. i want to how to write external devices register 40000. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/10/2019 12:52:16New subject after splitting |
|
10/11/2019 4:17 PM | |
Joined: 9/16/2013 Last visit: 1/5/2024 Posts: 511 Rating: (105) |
If device is a MASTER, it means you gonna be slave, device will ask you for your holding register (40000---). In that case you need to use MB_MASTER FB inside s71200. Take a look at picture. But it is more likely that you are Master and Device is a slave, since you need to write something on device registers, in that case u need to use MB_CLIENT. |
Last edited by: SOble at: 10/11/2019 16:18:06Website: |
|
Follow us on