4/3/2015 11:27 AM | |
Posts: 8 Rating:
|
Thank you so much ixo65. It works great. I´m now trying to expand my program for temperature steps. Like this: Press I1 warms the water to 60 degrees. When reached and press I2 these steps kicks in: 60 degrees for 30 minutes 70 degrees for 30 minutes 80 degrees for 10 minutes I have done a program but I´m having troubles with steps kicking in when they are not supposed to do. I Think I can solve it but maybe I´m doing it more complicated than it is. Thanks for all help. /m AttachmentDBB Bryggverk.zip (45 Downloads) |
4/3/2015 6:02 PM | |
Joined: 12/18/2014 Last visit: 1/25/2021 Posts: 20987 Rating:
|
Here is the program in FBD. If you have any questions, just ask. AttachmentDBB_Bryggverk_FBD.zip (53 Downloads) |
4/3/2015 9:05 PM | |
Joined: 12/18/2014 Last visit: 1/25/2021 Posts: 20987 Rating:
|
Excuse me, but I forgot after the simulation change the time ranges of the timers back to minutes. |
4/5/2015 8:34 PM | |
Posts: 8 Rating:
|
I can´t thank you enough. I´ll send you some beer when it´s all done :) |
This contribution was helpful to
1 thankful Users |
4/24/2015 11:11 PM | |
Posts: 8 Rating:
|
Hi again, I have now programmed my beer machine so I can set the parameters from the display. I´m using Mathematic Instructions to the different temperature steps. So when I want the first step to be 72 degrees I set the temperate I want in the display and then the values for the other heats sets automaticly to 70 and 71 degrees. It works fine but I have one problem.The mathematic instructions are not connected to outputs and I can´t transfer the program to the PLC unless the are connected. I have twelve mathematic instructions and not enough analog flags to connect to. What to do? I attach the program. / Mikael AttachmentDBB Bryggverk 2 test2.zip (44 Downloads) |
Last edited by: aoke_frivall at: 4/24/2015 11:12:39 PM |
|
Follow us on