(0)| 3/16/2013 3:02 PM | |
|
Posts: 1742 Rating:
|
Hello, The 1AE31 version is corresponding to the versin V3.0 of S7-1200. See http://support.automation.siemens.com/WW/view/en/61777437 They list the requirements: Requirements to be able to use the described functionalities: SIMATIC S7-1200 with firmware version 3.0 and higher STEP7 Engineering System version V11 SP2 Update3 and higher; see entry ID 56771572 Hardware Support Packages for S7-1200 FW3.0 54164095The HW suppport package is to be installed in Step7. To install a Support Package, follow these steps: 1. Click "Support packages" in the "Options" menu. The "Detailed information" dialog opens. A table lists all support packages from the directory that you selected as the storage location for support packages in the settings. 2. If you want to install a support package that is not in the list, you have the following options: – If the support package is already on your computer, you can add it to the list by selecting "Add from the file system". – If you add a support package from the "Service & Support" page on the Internet, first you download it by selecting "Download from the Internet". Then you can add it from the file system. 3. Select the support package that you want to install. 4. Click "Install." 5. Close and then restart the TIA Portal. |
| 3/16/2013 3:02 PM | |
|
Joined: 8/31/2010 Last visit: 12/6/2025 Posts: 1525 Rating:
|
Hello the_passerby, You need STEP 7 v11 HSP to get the 6ES7212-1AE31-0XB0 in the Hardware Catalog of your STEP 7 v11. Download: STEP 7 (TIA Portal) V11 Support Packages for the hardware catalog in the TIA Portal FAQ: How can you update the hardware catalog in STEP 7 (TIA Portal) V11? |
|
Like it? Rate it! |
|
Follow us on