10/2/2014 7:32 AM | |
Joined: 10/11/2006 Last visit: 4/18/2024 Posts: 5819 Rating: (787)
|
Hello, please see the commissioning manual: http://support.automation.siemens.com/WW/view/en/99687313 |
With best regards, |
|
This contribution was helpful to1 thankful Users |
5/3/2016 10:09 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Please read below thread for information. problem about AC SERVOMOTORPlease provide the MLFB number on the control card of 611 drive which shall help to identify if it is 611U or 611D. HTH. Hello, Please read below thread & see the attachment there from Mr. Dave. I would recomend you to get this motor repaired at nearest Siemens service support center, since encoder alignment job is very precision. encoder alingment in servo motors |
Last edited by: PISCEAN 2010 at: 5/3/2016 10:49:34 AM |
|
5/7/2016 11:40 AM | |
Joined: 10/13/2013 Last visit: 7/21/2021 Posts: 43 Rating: (0) |
hello There is attached file includind some image of simodrive. I hope it will be help. thanks & best regards AttachmentDoc1.pdf (397 Downloads) |
Last edited by: Min_Moderator at: 5/9/2016 1:22:04 PMConvert docx to pdf |
|
Follow us on