8/12/2015 7:08 AM | |
Posts: 23 Rating: (0) |
hi dear. how install liberary s7 200? and can i connect to s7 200 with windose 7 64 bit or 32 bit ? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/12/2015 11:10:47 AMNew subject after splitting |
|
8/12/2015 11:45 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi yasin, yes, you can connect to S7-200 with Win7 32/64bit. But you need to install the latest Micro/Win-Version STEP7 MicroWIN V4.0 SP8 and SP9If you already have installed the latest version, there maybe could be a problem with communication drivers. See following Thread to fix it. At the very end of the first page there is a file in the attachment.PG/PC Interfacehope this helps,regards, |
FCK WAR! |
|
Follow us on