12/18/2018 12:12 PM | |
Joined: 12/18/2018 Last visit: 5/29/2024 Posts: 27 Rating: (0) |
Hello Dear Sir, Thank you for your support I need to change p492, p1590[0], p1592[0], p1752[0], p1757[0], p3843[0] parameters, because, we have same pumps with same induction motors but one of them some times trip, when I check the parameters I found that the parameters are not same.But I could not changed them, because these parameters are absent in the expert list. (see attached pic and excel file) p492, p1590[0], p1592[0], p1752[0], p1757[0], p3843[0] please help how to change these parameters. (see Qqq.zip file CU2 Project file ) exported file With Best regards Batyrbek Allashov Attachment171218.zip (240 Downloads) |
12/19/2018 7:32 AM | |
Joined: 12/18/2018 Last visit: 5/29/2024 Posts: 27 Rating: (0) |
Thank you for support Please, Could you help me to change the parameters, as in the comparison list in our project, except those marked with a marker, since I cannot use access level 4. I compared an asynchronous motor with these parameters, working properly without any overcurrent trips. Why do I consider shutdown due to overcurrent due to parameters, we replaced the asynchronous motor, checked the power cables, but the shutdown due to overcurrent still occurs With Best regards Batyrbek Attachmentto support.zip (234 Downloads) |
Follow us on