5/23/2014 10:37 AM | |
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating: (23) |
I think this is what you are looking for. Siemens have in built software for Energy Management. Have a look. |
5/23/2014 1:19 PM | |
Posts: 46 Rating: (0) |
Hi, I know about that, but I was wondering can I use my existring equipemnt in this softvare?
|
5/23/2014 1:20 PM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308) |
Hello Siemens has these standard packages for Energy Management : SIMATIC B.Data SIMATIC Powerrate Here is the link : Software for Energy Management Besides, if you are familiar with STTEP7 and WinCC then it is easy to create your own customised package. SIMATIC B.Data can acquire raw energy data from WinCC / OPC and provide detailed reports and analysis. Maybe this is what you are looking for. Hope this helps Cheers Navnag |
Last edited by: Navnag at: 5/23/2014 1:22 PMThere is no such thing as the last bug in a program |
|
5/26/2014 8:19 AM | |
Posts: 46 Rating: (0) |
Hi, do I must have WINCC Powerrate to be able to work with B.Data? Or can I use my WinCC Advanced ?
|
5/26/2014 9:21 AM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308) |
Hello SIMATIC B.Data Acquisition server supports data Acquisition from the following : a) WinCC Professional ( With or without Power Rate ). If you use Power rate then you have more features. By default B.data Acquired data from WinCC Compressed Archives ar 15 Min intervals ( Adjustable ) b) OPC Server DA2.0 Compatible OPC Serevr c) Oracle SQL Server d) FTP Server ( ASCII ) I am attaching here an Extract from B.Data Manual, which will provide you mode information Hope this helps Cheers Navnag AttachmentBData_Requirements.pdf (330 Downloads) |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
Follow us on