(0)| 12/11/2007 7:27 AM | |
|
Joined: 10/11/2006 Last visit: 12/22/2025 Posts: 6062 Rating:
|
Hello Maris, first the guide from changing over from CU2 to CUVC. You can use the old T100 also together with the CUVC board. It is not possible to download T100 parameters to the CUVC. Of course for new applications, it would mostly not be necessary to have a T100 board together with CUVC (assuming that the program on T100 is standard MS100 "free blocks"), cause the CUVC itself has free blocks available. In your case, I would recommend to use the T100 as before and set the communication between T100 and CUVC according to the CU2's parameterization. Attachmentguide_cu2_cuvc.pdf (962 Downloads) |
|
With best regards, |
|
| 5/3/2017 3:13 PM | |
|
Posts: 4758 Rating:
|
New question published by Master drives is split to a separate thread with the subject Simovert VC 6SE7023 T100 board, inverter is showing A100. Best regards |
| 5/8/2017 12:56 PM | |
|
Posts: 3 Rating:
|
I am also facing the same problem . how to copy T100 configuration parameter ? Is it possible through Drive monitor ? If yes how ? |
Follow us on