3/15/2012 12:05 PM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello R&R, You have to Upgarde in two Step 1. V6.X to V7.1 2. V7.1 to V8.0 Detail About the upgarde SIMATIC PCS 7 engineering systems with Engineering Software V6.x or V7.0 can be upgraded to Version 7.1 using the SIMATIC PCS 7.1 Engineering Upgrade Package. The SIMATIC PCS 7 Engineering Upgrade Packages V6.x to V7.1 and V7.0 to V7.1 are each available in two versions: • SIMATIC PCS 7 Engineering Upgrade Package AS/OS, 250 to 2 000 POs (with OS Runtime license for productive operation) • SIMATIC PCS 7 Engineering Upgrade Package AS/OS, unlimited POs (with OS Runtime license for productive operation) Engineering Upgrade Package V7.0 to V7.1 The licenses included in the Engineering Upgrade Package V7.0 to V7.1 apply to the following software components of SIMATIC PCS 7 version 7.0: • PCS 7 Engineering AS, OS, AS/OS (250 POs to 2 000 POs)1) or PCS 7 Engineering AS, OS, AS/OS (POs unlimited)1) • PCS 7 Import/Export Assistant • Version Cross Manager • Version Trail • PCS 7 SFC Visualization • WinCC Redundancy • PCS 7 AS Runtime License (AS Runtime PO) • PCS 7 BCE • SIMATIC NET S7-1613 for Industrial Ethernet Engineering Upgrade Package V6.x to V7.1 The licenses included in the Engineering Upgrade Package V6.x to V7.1 apply to the following software components of SIMATIC PCS 7 version 6.0/6.1: • PCS 7 Engineering AS, OS, AS/OS (250 POs to 2 000 POs) or PCS 7 Engineering AS, OS, AS/OS (unlimited POs) • PCS 7 Import/Export Assistant • Version Cross Checker • Version Trail • PCS 7 PID-Tuner • PCS 7 SFC Visualization • WinCC Redundancy • PCS 7 BCE • SIMATIC NET S7-1613 for Industrial Ethernet Note: The PO Upgrade licenses included in the SIMATIC PCS 7 Engineering Upgrade Package V6.x to V7.1 convert the POs of the CFC licenses counted in SIMATIC PCS 7 V6.x into AS Runtime licenses. Corresponding to the scope of the CFC license of your PCS 7 Engineering Software V6.x (250 POs, 1 000 POs, 2 000 POs, 3 000 POs, 5 000 POs or 8 500 POs), you thus have the identical number of AS Runtime POs in each case for AS Runtime operation following the upgrade to V7.1. You will Find all the Information In the PCS7 Catalog Dec. 2011 www.siemens.com/industrymall Also Have a look on SIMATIC Process Control System PCS 7 Software update with utilization of new functions SIMATIC Process Control System PCS 7 Software update without utilization of new functions |
Ammy |
|
This contribution was helpful to1 thankful Users |
Follow us on