5/25/2012 10:07 AM | |
Posts: 3037 Rating: (192)
|
Hello, You have not any possibility to log data with KTP 600. What are the functional differences between the different SIMATIC panels? You need another panel for this, for example a TP277 or OP277. Tweety |
This contribution was helpful to1 thankful Users |
5/29/2012 1:36 PM | |
Joined: 2/16/2011 Last visit: 4/4/2024 Posts: 229 Rating: (27) |
Hello Tiago, First: 2 arrays (31 Int * 12 months * 2 array * 5 years) = 3720 Int's = 7440 Bytes the 1212 has 25K work memorie, then it's OK. If you want to store more data you can use the load memorie 1MB. You can use dataloggin aplication in CPU to store the data, but you can't retrieve the grafic in KTP basic, only in MP's and Konfort panels. But you can get the data with a PC. Pegaia's Sample program: S7-1200 and DATA LOGIf you prefer you can custumize the webpage from the CLP webserver. Regards.
|
Gabriel de Oliveira |
|
5/29/2012 1:40 PM | |
Joined: 2/16/2011 Last visit: 4/4/2024 Posts: 229 Rating: (27) |
Hello again, You can find more information inS7 1200 forum Regards
|
Gabriel de Oliveira |
|
5/30/2012 4:32 PM | |
Posts: 10 Rating: (1) |
Hello, Thank you so much for the info and help. I'll see if i can get it done
I will check it as soon as possible. Many thanks.
Hi, Sorry for posting in the wrong forum. I'll most likely use FW 2.0 (don't have access to a MMC card right now and i really need to finish this project) with STEP 7 v11 update 3.. Is it 100% compatible or will i have some problems? Thank you |
Follow us on