10/26/2013 8:57 AM | |
Posts: 5 Rating: (1) |
Hi., other option is Data block..... if use Data block means the values are stored in Data block...... |
10/26/2013 9:11 AM | |
Posts: 10 Rating: (0) |
Hi Scan, Ok...Thank you very much - i'll try to use Data Block. But is there way to access data of data block from WINCC tags BR |
10/26/2013 10:08 AM | |
Posts: 5 Rating: (1) |
Hi, if u have use tia portal means plc tag are easy to access in wincc tags |
10/26/2013 3:21 PM | |
Posts: 10 Rating: (0) |
Thank's Ganes10, comment to Your comment, So, for example i have one functional block FB50.
So in FB50 i have some in's and out's with init values. Then i put to my OB1 two blocks of FB50, and automatic create INSTANCE DB50 and DB51 for its. Then i want to change init values in DB51 - because algorithm of FB50(DB51) is some another, than FB50(DB51). But "Inital Values" field is disable ("gray"). So if i true understand??? - i must additional to create two SHARED data blocks (DB60 and DB61) with init values, and every of pins FB50, which i want to be with init value, connect to correspond variable from DB60 (for FB50(DB50)) or DB61 (for FB50(DB51)). Sorry for my English BR |
10/27/2013 4:13 PM | |
Joined: 8/31/2010 Last visit: 5/15/2024 Posts: 1510 Rating: (222) |
Hello Sasha1981, You are welcome. You can change the init values not in the Instance Data block of your FB50, whereas you can edit them directly in your interface of FB50. Hope this helps. |
Like it? Rate it! |
|
10/27/2013 4:30 PM | |
Joined: 8/31/2010 Last visit: 5/15/2024 Posts: 1510 Rating: (222) |
Hello BR, If you are using WinCC Classic (v7.x) make use of How do you integrate an existing WinCC project into a STEP 7 project? If you are using WinCC on TIA Portal then refer - SIMATIC S7-1200: AT 4 - Simple HMI Automation Tasks in 10 minutes or less |
Like it? Rate it! |
|
10/27/2013 8:18 PM | |
Posts: 10 Rating: (0) |
Hi Ganes10 Sure, I can change Init values for FB50. If I true understand You mean, that in OB1 I must open FB50 (right click-->Called Block-->Open) and in block interface set some init values. BUT! After change some init values for this FB50, all FB50’s in OB1 need for update, because project will be incorrect. So after update all blocks is good, but in equal init values - I want for different init values. So, I think, that there are must be some another blocks for inits. Elements of structure of this block I must connect to correspond variable of every FB50 in OB1. BR |
Follow us on