Industry Online Support
Technical Forum
9/7/2009 5:17 PM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (172) |
For me it seems to be the language of the operating system, as you thought. The problem is, that not the language settings cause this problem, it's the version of the operating system. It is a difference whether you use an french windows or an english version set to french language options. The problem is known, see FAQ http://support.automation.siemens.com/WW/view/en/23568401 Microsoft has such problems, too,see http://support.microsoft.com/kb/292582/en-us Either you can solve it with this or you hve to reinstall Windows as the path itself (it's an system variable) contains characters the setup doesn't support. Hope you can solve it by editing the settings for the path variable. Please note that this problem is not specific to Siemens software, it might appear with every product, as you can see from MS software products, too. |
Have Fun! |
|
Follow us on