6/5/2020 4:15 PM | |
Joined: 3/11/2015 Last visit: 4/16/2024 Posts: 68 Rating: (1) |
Hi, how to resolve it, i have installed WinCC RT Advanced V13 SP1 Upd9 & no interfaces are available in Set PG/PC, & the Service which you mentioned is also not available. Kindly let me know if you have any suggestions. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/08/2020 08:31:43New subject after splitting |
|
6/12/2020 10:05 AM | |
Joined: 8/3/2009 Last visit: 4/23/2024 Posts: 12834 Rating: (1639)
|
Hello perhaps you have to initialize the Interface again: https://support.industry.siemens.com/cs/ww/en/view/11870489 Bye Murof |
If this Information really helps, you could use the Rate function |
|
6/18/2020 2:26 PM | |
Joined: 3/11/2015 Last visit: 4/16/2024 Posts: 68 Rating: (1) |
Hello, Yes, I have gone through this link before seeking help here, but it didn't work for me, the "Install/Remove Interfaces" were empty & since it is Windows 7 Ultimate, tried even deleting "data" folder despite having all interfaces in it. By the way Thanks, time being I have restored to earlier Automatic Restore point & now its working fine. Regards, Anandhakumar |
Follow us on