3/9/2016 7:20 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926) |
Hi Berg, In WinCC TAG management, in the "internal" section, you can go to the columns (Name, Data type, Length etc) and right click. Then you can go to Unhide->Value. There is a column added where you can see the actual value. Is this what you mean?? |
If I could help you, you can use the RATE button. Thank you. |
|
3/9/2016 2:13 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926) |
Hi Berg, You need to right click on one the columns in TAG management, not on the internal tag. With columns I mean: Name, Type, Parameters, Last Change. |
Last edited by: Oreca at: 3/9/2016 2:13:56 PMIf I could help you, you can use the RATE button. Thank you. |
|
3/9/2016 2:47 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926) |
Hi Berg, See attachment Is it now clear? I hope so..... Attachmenttag.zip (48 Downloads) |
If I could help you, you can use the RATE button. Thank you. |
|
3/9/2016 3:55 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926) |
Oh, Next time when you ask a question, please post the current PCS7 version you are working with (and Windows version if needed). Sorry, I assumed it was PCS7 8.0/8.1 I have to check how it was in v7.0For now: You can insert a IO field and connect the internal tag and you can view it in runtime. |
Last edited by: Oreca at: 3/9/2016 4:15:08 PMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
3/11/2016 9:29 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926) |
Hi Berg, Did you try to use a IO field in runtime by connecting the internal tag, so you can readout the value? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on