2/9/2018 10:19 AM | |
Joined: 1/12/2016 Last visit: 3/18/2024 Posts: 42 Rating: (4) |
Here are both project. Could you check it? --deleted Link-- Thanks a lot. AttachmentFiles.fm_2018-02-09_qcchu5y8.zip (150 Downloads) |
Last edited by: Jen_Moderator at: 2/9/2018 11:34:08 AMDeleted link and added file as an attachment. |
|
2/9/2018 10:29 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
hi, in the projects it looks ok. Regards Christoph |
2/9/2018 10:48 AM | |
Joined: 1/12/2016 Last visit: 3/18/2024 Posts: 42 Rating: (4) |
Still error. |
2/9/2018 10:55 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
check the entries in the log, there is a entry with text abort in line 8 |
2/9/2018 12:21 PM | |
Joined: 1/12/2016 Last visit: 3/18/2024 Posts: 42 Rating: (4) |
Yes, only 1 cable. I have log from S7-1500 only. S7-300 is in system fault, therefore I cant see diag. buffer. I guess S7-1500 cant reach S7-300 because it is in SF, but it goes to SF immediately after I make it IO Device. AttachmentDiagnostics.txt (133 Downloads) |
Follow us on